Keysight Oscilloscope Glossary

What is a Magnetometer?

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

What Is a Magnetometer?

A magnetometer is a scientific instrument used to measure the strength and direction of magnetic fields. You can find them in a wide range of fields, including geology, geophysics, archaeology, and aerospace engineering. The basic principle behind magnetometers is that they detect variations in the Earth's MF (magnetic field) and changes in objects made from ferromagnetic materials such as iron.

The three most common types of instruments in geophysical surveys are fluxgate, proton precession, and optically pumped magnetometers.

 

Magnetometer TypeExplanation

Fluxgate magnetometers

Used for measuring the Earth's MF, fluxgate sensors consist of coils of wire surrounded by a ferromagnetic core. As the MF changes, the core becomes magnetized, which induces an electric current in the coil. By measuring the strength of this current, you can determine the magnetic field strength.

Proton precession magnetometers

These magnetometers are more sensitive than fluxgate instruments and can detect small changes in Earth's MF. Proton precession magnetometers use the nuclear magnetic resonance of hydrogen atoms to measure magnetic fields. These instruments are often used for archaeological sites to locate buried structures or artifacts that contain magnetic materials.

Optically pumped magnetometers

Using lasers to measure extremely low-level fields, these instruments are extremely sensitive. They can detect small changes in the Earth's MF, such as those caused by solar storms. They are often used in aerospace engineering to measure a spacecraft's or satellite's orientation relative to the Earth's MF.

 

Key Takeaway
A magnetometer is a scientific instrument used to measure magnetic fields. It can detect and measure the strength, direction, and changes in magnetic fields. They are used in various applications, including navigation, geophysics, and materials science.

Buy Oscilloscopes at a Great Discount

  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

What Is a SQUID?

Superconducting Quantum Interference Device (SQUID) magnetometers are the most sensitive instruments available for measuring magnetic fields. SQUID magnetometry uses a superconducting quantum interference loop to measure minute changes in the Earth's MF, such as those caused by solar storms or internal geophysical processes.

You can use SQUIDs in various applications, including

Quantum Interference Devices have revolutionized the study of magnetic phenomena and have enabled the detection of previously undetectable magnetic signals.

However, SQUIDs are noise-sensitive instruments that require extremely precise measurements. This makes them difficult to operate, and they are usually only used in specialized laboratories.
 

What Is the Hall Effect?

The Hall effect is a fundamental physics phenomenon discovered by American physicist Edwin Hall in 1879. It refers to creating a voltage difference (known as Hall voltage) across a conductor or semiconductor material when the applied magnetic field is perpendicular to the current flowing through the material.

The Hall effect occurs because the magnetic field exerts a force on the material's moving charge carriers (usually electrons), causing them to deflect from their straight-line path. 

This deflection creates a buildup of charge on one side of the material and a deficit of charge on the other side, resulting in an electric field that opposes the deflection of the charge carriers. The electric field creates a voltage difference across the material, measured as the Hall voltage.

The Hall effect has many practical applications. For example, it measures magnetic fields, as in the case of Hall effect sensors. These sensors consist of a thin layer of semiconductor material with an electrical current passing through it. When a magnetic field is applied perpendicular to the current, the measured Hall voltage can determine the strength and direction of the field.

The Hall effect is also important in studying materials with electronic properties, such as metals, semiconductors, and superconductors. Scientists can gain insights into their electronic structure and behaviour by examining the Hall effect in these materials.
 

What Is a Magneto Induction Method?

The magneto-induction method is a geophysical exploration technique that measures the Earth's MF variations caused by subsurface magnetic materials. It uses an exciter current that generates a low-frequency magnetic field, which is proportional to the distance between the probe and the material under investigation. In geophysics it is used to measure the magnetic field strength at various locations on the Earth's surface. The data is then used to create a map of the magnetic properties of the subsurface.

The theory behind the magneto-induction method is that rocks and minerals have different magnetic properties that affects the Earth's MF. Some rocks and minerals, such as magnetite, are naturally magnetic, while others can become magnetized in a magnetic field.

In the magneto-induction method, a magnetic field source, such as a current-carrying loop, induces a magnetic field in the subsurface. The induced magnetic field causes a variation in the surface MF, measured by a magnetometer at the surface. 

The magneto-induction method has many applications, including mineral exploration, geothermal exploration, and environmental studies. It is often used with other geophysical exploration techniques, such as seismic and gravity surveys, to provide a complete picture of the subsurface.

What Is VSM?

VSM stands for Vibrating Sample Magnetometer, a type of scientific instrument used for magnetic measurements of different properties in materials. It is a highly sensitive and precise instrument that can detect tiny changes in magnetic fields.

The VSM works by vibrating a sample of the studied material in a magnetic field and measuring the resulting magnetic response. The sample is typically a small piece of the material, such as a thin film or a powder. 

The sample material is attached to a vibrating rod and placed in a magnetic field generated by an electromagnet. The vibrating sample generates a small alternating magnetic field measured by a sensor, such as a Hall sensor or a magnetic field sensor (magnetometer).

By measuring the magnetic response of the sample at different magnetic field strengths and directions, the VSM can determine the material's magnetic properties, such as its magnetic moment, coercive field, and magnetic susceptibility

These magnetic measurements provide information about the material's behaviour in different fields and are used to understand its magnetic properties.

The VSM is used in materials science research, particularly in studying magnetic materials, such as ferromagnetic, antiferromagnetic, and paramagnetic materials. It is also used in producing magnetic materials, such as in quality control and developing new magnetic materials.
 

How To Calibrate a Magnetometer?

Calibration of magnetometers involves correcting errors or offsets in their measurements to provide accurate readings. Here are the general steps for calibrating a magnetometer.

 

  1. Place the magnetometer in a known magnetic field. Do this by using a calibration source, such as a Helmholtz coil, or by placing the magnetometer near a known magnetic source, such as the Earth's MF.
  2. Record the raw data from the magnetometer, including the three components of the magnetic field (x, y, and z) and any offsets or noise.
  3. Analyze the data to determine any offsets or noise in the measurements. Do this by calculating the mean and standard deviation of the data and comparing it to the expected values.
  4. Apply corrections to the magnetometer to remove any offsets or noise. Do this by subtracting the mean or using more complex correction algorithms.
  5. Repeat the calibration process at different orientations and locations to ensure the magnetometer is accurate under different conditions.
  6. Validate the calibration by comparing the magnetometer readings to those of a known magnetic source or other magnetometers.

Browse Oscilloscopes at a Great Discount

  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Keysight Oscilloscopes

When it comes to tech equipment, you want the best of the best. That's why Keysight oscilloscopes are the perfect choice for your needs. With industry-leading performance, they're the ideal tool for many applications. 

From basic signal analysis to complex measurements, Keysight digital oscilloscopes have you covered. With models ranging from entry-level to high-end, there's a Keysight oscilloscope that's perfect for your needs. So why settle for anything less? See Keysights Used Equipment to find a wide variety of oscilloscopes to fit your needs.

Did you like this article?

Popular Used Oscilloscopes

Keysight Used Oscilloscopes offers a wide range of industry leading pre-owened oscilloscopes, ranging from older generation Agilent oscilloscopes to the newest Keysight oscilloscope models. So whether you are a fist time buyer, replacing a model like-for-like or looking for upgrade – we have something for you.

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.