How Does an Oscilloscope Work? – An In-depth Exploration for Engineers

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Can you imagine electrical engineering without oscilloscopes? Likely not. Oscilloscopes serve as the "eyes" for engineers, providing indispensable insights into electronic signals. These tools not only offer a visualization of waveforms but also present a broad spectrum of measurement and analysis capabilities.

Picture this: You're working on an intricate embedded system, and after weeks of development, the moment of truth arrives — it's time to test. 

You power up the system, but instead of a smooth operation, the device behaves erratically. Panic sets in. 

Traditional multimeters and logic analyzers offer limited help. You plug in an oscilloscope and immediately discover that a certain signal is dropping out at irregular intervals. 

You trace the issue back to a faulty capacitor that's messing up your power supply line. Without the oscilloscope, diagnosing this problem could have taken days or even weeks. 

So, how does this extraordinary tool manage to provide such crucial data? Let's dive in.

A Quick Refresher: The Oscilloscope's Place in Electrical Engineering

Oscilloscopes have come a long way since their inception in the early 20th century. Initially, they were analog devices with limited capabilities, primarily used to display simple waveforms. 

As technology advanced, digital storage oscilloscopes took the stage, offering unprecedented features like data storage, advanced triggering, and complex signal analysis. 

Today, the modern oscilloscope serves as a multi-functional tool, capable of meeting the demands of sophisticated engineering projects.

Multifaceted Roles of an Oscilloscope

  • Signal visualization: Provides a graphical representation of electrical signals, making it easier to understand their behavior over time.
  • Time and frequency measurements: Helps to measure the period, frequency, and pulse width of signals, serving as a critical tool in designing and debugging circuits.
  • Anomaly detection: Facilitates the identification of signal anomalies such as noise, jitter, and glitches, thus aiding in quick troubleshooting.
  • Complex analysis: Supports FFT (Fast Fourier Transform) and other mathematical operations to analyze the frequency domain and phase relationships.
  • Digital protocols debugging: Decodes various digital protocols like SPI, I2C, and UART, streamlining the development of digital systems.
  • Calibration and verification: Validates the performance of other devices, ensuring that components and systems meet specified criteria.
  • Education and training: Acts as a foundational instrument for students and young engineers, providing hands-on experience with electrical and electronic concepts.

Understanding the roles that oscilloscopes play in electrical engineering helps you appreciate the instrument's versatility and indispensability. Armed with this knowledge, let's explore how an oscilloscope actually works.

The Core Components and Their Functions

An oscilloscope comprises various components, each serving a unique function to deliver that intricate view of electrical signals. Understanding how each part works helps you use this tool efficiently.

Display

The display serves as the window into the electrical world, showing you the shape, frequency, and other characteristics of your signal. 

In analog oscilloscopes, a CRT display uses electron beams to draw waveforms on a phosphor screen. In contrast, digital oscilloscopes rely on modern LCD or LED screens, which offer better resolution and features like color coding, annotations, and even touch control.

Vertical Controls

Vertical controls let you zoom in and out on the amplitude of the signal, allowing for detailed inspection. By adjusting the volts per division (volts/div), you can make subtle or significant changes to the waveform's vertical display. 

This ability is crucial for tasks such as verifying amplitude levels, detecting overshoot, or measuring the voltage between any two points on the waveform.

Horizontal Controls

Horizontal controls help you scrutinize the time domain aspects of your signal. You can change the time per division (time/div) setting to stretch or compress the waveform horizontally. 

This manipulation allows you to examine specific sections of the signal more closely. It's particularly useful for looking at the timing of events in a signal sequence or understanding the frequency content.

Triggers

Triggering is perhaps one of the most critical features in an oscilloscope, dictating when and how the device captures the data.

Basic triggers, often found in analog oscilloscopes, usually capture the signal when it crosses a specified voltage level. 

Digital oscilloscopes offer a plethora of advanced triggering options:

  • Edge triggering: Initiates capturing when the signal crosses a particular voltage level, similar to basic analog triggers but with more control.
  • Pulse triggering: Triggers the oscilloscope based on the duration of a pulse, useful for capturing anomalies like glitches or dropouts.
  • Runt triggering: Activates capture when the signal partially crosses a voltage threshold but doesn't go all the way through, identifying abnormal signals.
  • Logic triggering: Employs multiple conditions across different channels, offering a way to trigger on complex digital or mixed signals.

Understanding the intricacies of these trigger settings enables you to capture even the most elusive signals, thereby making your troubleshooting and analysis tasks significantly easier.

Analog Vs Digital Comparison

ComponentAnalog OscilloscopeDigital Oscilloscope
DisplayCRT (Cathode Ray Tube)LCD/LED Screen
Vertical ControlsPotentiometers usually control amplitudeDigital controls, often with touch capability
Horizontal ControlsControlled manuallyDigital controls, zoom and pan functionalities
TriggersBasic edge triggeringAdvanced triggers like pulse, runt, logic

Technology Behind Waveform Visualization

Analog Phosphor Displays

In analog oscilloscopes, the phosphor coating inside the CRT screen glows when struck by an electron beam, producing the visible waveform. The electron beam sweeps horizontally across the screen in sync with the input signal, creating a real-time, continuously updating display.

Modern Digital Screens

Digital oscilloscopes capture and store the waveform data first. Then, they process this data and display it on an LCD or LED screen. 

These digital displays offer multiple advantages, such as the ability to zoom, pan, and even perform mathematical operations on the displayed waveform.

The leap from phosphor displays to modern digital screens has not only improved resolution and flexibility but has also allowed for a variety of advanced functionalities that transform the oscilloscope into a comprehensive analysis tool.

Analog Oscilloscope

Analog oscilloscopes have a rich history, tracing their roots back to early 20th-century scientific research and World War II-era advancements. Initially used for radar and communication systems, their applications quickly expanded as the field of electronics evolved. 

While digital oscilloscopes have largely taken over, the principles behind analog oscilloscopes remain a fundamental part of the electronic measurement landscape.

Step-by-Step Signal Processing in an Analog Oscilloscope

  1. Signal input: Connect the probe to the circuit under test. The oscilloscope receives the electrical signal through its input terminal.
  2. Amplification: A pre-amplifier boosts the incoming signal. The vertical controls adjust the level of amplification.
  3. Attenuation: Optionally, you can attenuate high-voltage signals to bring them within a safe and measurable range.
  4. Vertical deflection: The amplified or attenuated signal then moves to the vertical deflection plates of the CRT. This causes the electron beam to move vertically.
  5. Horizontal sweep: A separate circuit generates a linear, time-based signal that controls the horizontal deflection plates.
  6. Electron beam movement: The simultaneous actions of the vertical deflection and horizontal sweep cause the electron beam to trace the waveform on the phosphor-coated screen of the CRT.
  7. Phosphor illumination: The moving electron beam strikes the phosphor, causing it to glow and thus visually represent the waveform.
  8. Retrace & reset: After plotting one sweep of the signal, the electron beam quickly returns to its starting position to begin the next sweep.

Capturing and Interpreting Electrical Signals

Analog oscilloscopes use the continuous motion of an electron beam to plot real-time signals. The electron beam moves across the phosphor screen horizontally at a constant rate, determined by the time/div setting. Simultaneously, the incoming signal influences the vertical deflection of the beam. 

Essentially, the horizontal movement represents time, and the vertical movement represents voltage, creating a real-time plot of voltage vs. time.

The trigger settings control when the horizontal sweep begins, thereby capturing the waveform at a consistent point in its cycle. This ensures that the waveform appears stable on the display, allowing you to make accurate time and amplitude measurements.

While analog oscilloscopes may not offer the digital storage, complex triggering, or signal analysis capabilities of their modern counterparts, their real-time, analog display can be invaluable for capturing rapidly varying or transient signals. 

Understanding these foundational principles not only helps us appreciate the technological evolution but also enriches our grasp of current oscilloscope technology.

Digital Oscilloscope

The advent of digital technology has revolutionized the world of oscilloscopes, enabling more precise measurements, more features, and greater flexibility. 

How Digital Oscilloscopes Process Signals

In a digital oscilloscope, the signal pathway starts similarly to that of an analog one—with a probe connected to the circuit capturing the electrical signal. However, from here on, the process takes a digital turn. 

The incoming analog signal passes through an Analog-to-Digital Converter (ADC) that samples the signal at discrete intervals and converts it into digital values. The oscilloscope then stores these digital values in memory for further processing or display. This allows for intricate manipulations, from mathematical operations to advanced triggering, before rendering the final waveform on the screen.

Key Benefits and Enhanced Features of Digital Oscilloscopes

  • Signal storage and retrieval: Unlike analog oscilloscopes, digital ones can store captured waveforms indefinitely, allowing for detailed post-capture analysis.
  • Advanced triggering: Sophisticated triggering options, such as logic, pulse width, and protocol-based triggers, allow for precise data capture.
  • Mathematical operations: You can perform operations like Fast Fourier Transform (FFT), integrals, and derivatives directly on the stored waveforms, enabling complex signal analysis.
  • Multiple channels: Digital oscilloscopes often come with four or more channels, letting you monitor multiple signals simultaneously.
  • High resolution and accuracy: Thanks to high-speed ADCs and greater bit-depth, digital oscilloscopes offer superior resolution and accuracy.
  • Zoom and pan: The ability to zoom into a specific part of a stored waveform and pan across it provides enhanced signal inspection capabilities.

Signal Capturing, Storage, and Resolution

Digital oscilloscopes excel in capturing, storing, and displaying signals:

  • Capturing: The ADC samples the incoming signal at a high rate, often in the gigasamples per second (GSa/s) range. The higher the sampling rate, the more accurately the oscilloscope can represent fast-changing signals.
  • Storage: Once sampled, the oscilloscope stores these digital points in its memory. This storage capability enables post-capture analysis and allows you to scrutinize a waveform long after removing the signal input.
  • Resolution: Digital oscilloscopes often have a high bit-depth—ranging from 8 to 16 bits or more. Higher bit-depth results in greater vertical resolution, making it easier to distinguish small signal details.

The evolution from analog to digital oscilloscopes represents a technological leap that has expanded the tool’s versatility and precision. Today, a digital oscilloscope is not just an instrument for viewing waveforms but a comprehensive platform for complex electrical signal analysis and troubleshooting.

Signal Probing and Measurement Techniques

Choosing the right probe for your oscilloscope is like selecting the right lens for your camera—it's crucial for capturing accurate and meaningful data. A poorly-matched probe can distort the signal, compromise measurement accuracy, or even risk damaging the circuit under test. With a myriad of probes available, understanding the strengths and limitations of each is essential.

Types of Probes and Their Applications

Probe TypeKey CharacteristicsIdeal Scenarios
Passive ProbesSimple, reliable, low-costGeneral-purpose, low-frequency applications
Active ProbesHigh bandwidth, low loading effectHigh-frequency, low-amplitude signals
DifferentialMeasures difference between two pointsEliminating common-mode noise
Current ProbesDirect current measurementCurrent profiling, inrush testing
High-VoltageBuilt for high input voltagesPower electronics, motor drives

Importance of Right Probe Choices for Accurate Measurements

The oscilloscope and probe work in tandem to measure a wide variety of signal attributes. Be it voltage, current, or more complex features like phase relationships, the right probe ensures that the oscilloscope interprets and displays the signal faithfully.

Common Measurements and Their Significance

  • Rise/fall time: Measures how quickly a signal transitions from a low to a high state or vice versa. Critical for assessing the speed of digital circuits.
  • Pulse width: Indicates the duration of a pulse within a signal. Essential for understanding pulse-driven or modulated systems.
  • Frequency: Shows how often a periodic event occurs within a specific time frame. Fundamental for tuning oscillators or assessing signal stability.
  • Phase angle: Measures the phase difference between two signals, which is important in applications like motor control or signal processing.
  • Peak-to-peak voltage: Measures the amplitude difference between the highest and lowest points of a waveform, useful for assessing signal strength or quality.

Selecting the right probe and knowing which measurements to perform empower you to harness the full capabilities of your oscilloscope. Whether you're debugging a new design or conducting in-depth research, these choices dramatically affect the quality and reliability of your data.

Cutting-Edge Features That Make Modern Oscilloscopes Indispensable

Modern oscilloscopes are not just signal display tools; they are comprehensive analysis platforms brimming with advanced features. These features significantly expand the oscilloscope's utility, making it indispensable for modern electrical engineering tasks. 

From FFT analysis to serial bus decoding, these functionalities add layers of depth to what you can accomplish with an oscilloscope.

Advanced Features in Contemporary Oscilloscopes

  • FFT analysis: Fast Fourier Transform (FFT) allows you to analyze the frequency components of a signal, offering a different perspective from the time-domain representation.
  • Serial bus decoding: This feature decodes data on serial buses like UART, SPI, and I2C directly on the oscilloscope screen, simplifying debugging and analysis of digital communication systems.
  • Advanced triggering: Beyond the basic edge triggering, modern oscilloscopes offer various advanced options such as pulse width triggering, runt triggering, and even protocol-based triggering.
  • Waveform math: Perform real-time mathematical operations on captured waveforms, including addition, subtraction, and multiplication, directly on the oscilloscope.
  • Cursor measurements: Cursors provide a straightforward way to measure various aspects of a waveform directly on the display, eliminating the need for manual calculations.
  • Automated measurements: Built-in software algorithms can automatically measure parameters like RMS voltage, peak-to-peak voltage, and rise time, making the process more efficient and accurate.
  • Mixed signal analysis: Some oscilloscopes offer both analog and digital channels, allowing for the simultaneous capture and analysis of both analog and digital signals.
  • Remote control and networking: Modern oscilloscopes often come with Ethernet ports and software that allows for remote operation, enabling distributed teams to collaborate more effectively.

These advanced features contribute to an environment where engineers can dig deeper into signals, troubleshoot more efficiently, and understand complex systems more thoroughly. 

FFT analysis opens up frequency-domain insights, while serial bus decoding simplifies the arduous task of interpreting digital data streams. 

Advanced triggering options allow for precise captures, and automated measurements speed up routine tasks. 

Together, these features elevate the humble oscilloscope from a mere display tool to a powerful analysis instrument.

Safety, Calibration, and Quality in Oscilloscopes

When using oscilloscopes, three key aspects can't be compromised: safety, calibration, and quality. These factors are not just add-ons; they are essentials for ensuring accurate measurements and preventing accidents during testing and troubleshooting.

Essential Safety Guidelines for Oscilloscope Usage

  • Ground connection: Always properly ground your oscilloscope to prevent electric shock and to ensure measurement accuracy.
  • Probe rating: Check the voltage and current ratings of your probe to ensure it is suitable for the circuit you are testing.
  • Avoid direct contact: Use proper clip attachments or probe holders to keep your hands away from live circuits.
  • Keep away from moisture: Never operate the oscilloscope in a damp or wet environment to avoid electrical hazards.
  • Regular inspection: Periodically inspect cables, probes, and connectors for signs of wear or damage. Replace them if needed.

The Importance of Calibration

Calibration maintains the accuracy and reliability of your oscilloscope. Inaccurate measurements can lead to flawed analyses, which can be costly and even dangerous.

Consistent calibration, usually done annually or as specified by the manufacturer, ensures that your measurements remain precise and reliable over time.

Keysight's Exceptional Quality Assurance

When it comes to quality assurance in oscilloscopes, Keysight Technologies sets the industry standard. With rigorous testing and quality control procedures, Keysight ensures that you are working with an instrument that not only meets but often exceeds industry standards. 

This commitment to quality brings unparalleled accuracy and reliability to your oscilloscope measurements, thereby making your investment in a Keysight oscilloscope a wise and long-lasting one.

Dive into Keysight's Used Oscilloscope Portfolio

  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Conclusion: The Oscilloscope – An Engineer's Trusty Companion

Understanding the intricacies of oscilloscope operation is not just an academic exercise; it's a practical necessity for any electrical engineer. From basic waveform visualization to advanced features like FFT analysis and serial bus decoding, the oscilloscope stands as a multifaceted tool that evolves with the complexity of modern engineering challenges.

The emphasis on safety, calibration, and quality underscores the meticulous nature of this instrument. It's not just about what you see on the screen; it's about knowing that what you see is accurate, safe, and of the highest quality.

"Precision in vision" is perhaps the most fitting phrase to describe the oscilloscope's role in refining engineering outcomes. When you work with an oscilloscope, you're not just tracing waveforms; you're peeling back layers of electrical behavior to reveal insights that can lead to innovation, solve complex problems, and improve system performance.

So, whether you're a seasoned engineer or a budding professional, an oscilloscope remains an invaluable companion. From waveform tracing to advanced analysis, oscilloscopes are, and will continue to be, at the heart of electrical engineering.

Final Key Takeaway: Embracing Innovation with Quality

In today's fast-paced world of electrical engineering, the blend of innovation and quality in modern oscilloscopes isn't just a luxury—it's a necessity. Using a Keysight oscilloscope means using a high-quality and advanced tool that combines innovation and quality control. 

It serves as both a testament to engineering prowess and a commitment to excellence, ensuring that you're not only keeping pace with technological advancements but also setting new benchmarks in reliability and precision.

Whenever You’re Ready, Here Are 5 Ways We Can Help You

  1. Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators.
  2. Call tech support US: 1 800 829-4444
    Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri
  3. Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
  4. Create an account to get price alerts and access to exclusive waitlists
  5. Talk to your account manager about your specific needs.

* Two weeks shipping time offer available for US customers only. Dependent on item availability and location