What is Vertical Division in Oscilloscopes?

This article is brought to you by the Keysight Used Equipment Store. The information applies to used and new equipment.

If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.

Your browser limits use of the Used Keysight Equipment website.
Please consider switching to a current version of Chrome, Firefox, Edge or IE11 to use this site.

Have you ever marveled at how a simple-looking tool like an oscilloscope can help decode the complex mysteries of electronic signals? This versatile tool has been at the heart of groundbreaking discoveries and innovations since it’s invention in 1893. 

Vertical division is a key feature that makes an oscilloscope essential for electrical engineers and professionals in related fields. This feature not only helps visualize but also analyze the properties of electrical signals. Today, we will delve deeper into vertical division and why it holds an important place in the use of oscilloscopes.
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
Vertical Division in Oscilloscopes: An Overview of Oscilloscope Graticule

The oscilloscope screen displays a grid, also known as a graticule. This grid consists of intersecting horizontal and vertical lines, creating small squares on the display. The purpose of the graticule is to measure the voltage (vertical axis) and time (horizontal axis) values of a waveform.

Vertical Division: Breaking it Down

Vertical divisions are the lines that span the vertical axis (y-axis) on an oscilloscope screen. Each division on this vertical scale represents a certain amount of voltage. This vertical scale is adjustable, allowing you to zoom in or out on the waveform for detailed analysis.

For example, if the vertical scale is set to 2 volts/division, then each vertical division represents 2 volts. A waveform that peaks at the second vertical division above the center represents a maximum voltage of 4 volts.

 

Key Takeaway
The vertical division in oscilloscopes is a foundational element that allows precise control over signal visualization, impacting the device's sensitivity, resolution, and advanced functions. Understanding and effectively leveraging it can greatly enhance signal analysis, and provide insights into both simple and complex waveforms.

Key Aspects of Vertical Division

Here's a snapshot of what vertical divisions facilitate:

  • Peak-to-peak voltage: The difference in voltage between the maximum positive and maximum negative peaks of a waveform.
  • RMS voltage: The effective value of an AC waveform. It is equivalent to the DC voltage that would provide the same amount of power to a load.
  • DC offset: The mean value of a waveform over a full period.

Sensitivity and Resolution

Controlling the sensitivity and resolution of an oscilloscope is a crucial aspect of signal analysis. Sensitivity, in the realm of oscilloscopes, is the capability to display low-level signals that are otherwise challenging to discern.

As you increase the sensitivity by reducing volts/division (volts/div), the minor signals in your measurement setup become magnified. Consequently, these small signals occupy more vertical divisions, resulting in improved visibility on the oscilloscope screen. This is especially important when working with signals of small amplitudes or when noise levels are comparable to the signal of interest.

The vertical scale setting also impacts the oscilloscope's resolution. The resolution is the smallest change in the input signal that the oscilloscope can detect. A lower volts/div setting allows the oscilloscope to visualize smaller changes in the input voltage. Understanding and adjusting the sensitivity and resolution effectively are essential in capturing and analyzing transient phenomena or detecting anomalies in the signal under study.

Complex Signal Measurement

The power of vertical divisions extends beyond simple voltage measurement and significantly aids in the visualization and analysis of complex signals. Oscilloscopes with more vertical divisions can more accurately represent intricate waveforms, leading to better precision in your measurements.

An oscilloscope with more vertical divisions can depict waveforms with higher vertical resolution, allowing for a more detailed analysis. For example, if you are examining a complex waveform consisting of numerous frequency components, the vertical divisions can help you distinguish between these components with greater clarity.

The additional visual resolution granted by more vertical divisions can help in distinguishing between closely-spaced voltage levels in digital signals. In the field of digital communications, this can be invaluable for decoding and analyzing digital protocols.

Understanding the full capabilities of vertical divisions also unlocks advanced oscilloscope functions. These include functions such as FFT (Fast Fourier Transform) that allow you to analyze the frequency components of your signal. By accurately capturing and displaying the time-domain signal, the oscilloscope can effectively compute the frequency-domain representation.

A Comprehensive Guide to Vertical Division Controls

Navigating the world of oscilloscopes often boils down to a basic understanding of key control features. Even though each oscilloscope model may have different labeling and organization of controls, the functionality of these crucial components remains consistent across models.

Volts/Div Control: Scaling the Vertical Grid

Volts/Div control, or the vertical scale control, is the knob that adjusts the value of each vertical division on the screen. This control is the key to tweaking the resolution and sensitivity of the oscilloscope. If you turn this knob clockwise, it generally increases the volts/div value. This action effectively decreases the vertical size of the waveform on the screen, causing the waveform to "shrink".

Conversely, turning the knob counter-clockwise reduces the volts/div value, "magnifying" the waveform vertically for detailed observation. By manipulating the Volts/Div control, users can adjust the oscilloscope to best suit the amplitude of the signal they are analyzing.
 

Vertical Position Control: Shifting Waveforms

The vertical position control is another essential knob that enables you to move the waveform vertically across the screen. This control is particularly useful when you are examining multiple waveforms simultaneously. 

When you  adjust the vertical positions, you can separate the waveforms to prevent overlap and ensure clear visibility of each waveform. This helps establish a baseline or reference point for comparing other waveforms or signal components.

Input Coupling Switch: Defining Signal Entry

The input coupling switch is a critical control that dictates how the signal enters the oscilloscope. The three common settings available are Direct Current (DC), Alternating Current (AC), and Ground (GND).

  • DC coupling allows both AC and DC components of the signal to pass into the oscilloscope. This mode is useful when you want to observe the total waveform, including any DC offset.
  • AC coupling blocks the DC component and only allows the AC component of the signal to pass. This is particularly beneficial when you want to observe AC signals superimposed on a high DC level without the DC offset skewing your view.
  • GND coupling disconnects the input signal and grounds the input of the oscilloscope. This mode is essential for setting baseline levels before making measurements and ensures the oscilloscope is functioning properly.
     

Table of Typical Vertical Division Settings and Applications

Vertical Scale (volts/div)Typical Applications
5 mV to 20 mVAnalysis of small signals, noise measurement
50 mV to 200 mVCircuit debugging, low voltage measurements
1 V to 5 VPower supply testing, medium voltage circuit analysis
10 V and aboveHigh voltage circuit testing, power analysis

Vertical Division in Advanced Oscilloscope Features

Vertical divisions play a significant role in the functionality of advanced oscilloscope features. Some oscilloscope models come equipped with sophisticated features that utilize the concept of vertical divisions in diverse ways, further magnifying their utility. 

Let's explore three of these advanced functionalities.

  1. Math functions: Oscilloscopes can perform mathematical operations on the input signals and display new waveforms derived from these computations. They can add, subtract, and multiply waveforms using vertical division measurements. Some oscilloscopes can even integrate or differentiate the input signals.

    The accuracy of these calculations is greatly dependent on the vertical scale set by the user. A finer vertical scale will result in more precise mathematical results. These math functions are particularly useful in comparing different signals or observing the effect of one signal on another.
     
  2. Automatic measurements: Automatic measurement functions are a powerful tool that oscilloscopes offer to quickly quantify waveform parameters. These include parameters like mean value, Root Mean Square (RMS) value, and peak-to-peak values. The oscilloscope calculates these values based on the vertical divisions.

    For example, to measure the peak-to-peak voltage of a signal, the oscilloscope counts the number of vertical divisions from the highest to the lowest point of the signal and multiplies it by the volts/div setting. This feature saves time and reduces human error in reading values off the graticule.
     
  3. Digital decoding: In the era of digital communication, the ability to decode digital signals is a must. Vertical divisions prove crucial in this aspect as well. Protocols like Serial Peripheral Interface (SPI), Inter-Integrated Circuit (I2C), and Universal Asynchronous Receiver-Transmitter (UART) have data represented by specific voltage levels.

    The oscilloscope decodes these protocols by distinguishing between these voltage levels, a task made possible by vertical divisions. Precise vertical scaling can help differentiate between voltage levels, especially in protocols with many levels, ensuring accurate decoding and analysis of digital communication.

Conclusion

Vertical divisions in oscilloscopes play a crucial role in bringing electrical signals to life, from simple waveform visualization to intricate signal analysis. They provide control over the sensitivity and resolution of the oscilloscope, empowering users to examine low-level signals and detailed aspects of complex waveforms. 

Mastering the use of vertical divisions on oscilloscopes opens up a world of deeper insights and precision. However, effective signal analysis doesn't rest solely on user proficiency but also significantly depends on the quality of test equipment used. Quality test equipment ensures accurate, reliable measurements, which are vital in fields where precision is paramount. 

This is where Keysight's Used Equipment comes in. Check out our extensive range of high-quality, pre-owned oscilloscopes and testing devices, like signal analyzers and network analyzers, each meticulously checked for quality and performance. Don't compromise on your pursuit of precision – visit the Keysight Used Equipment Store today.

Browse Oscilloscopes at a Great Discount
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
If you know which Keysight model is of interest to you and matches your technical requirements, visit the Used Equipment Store to see if you can save with our offers.
View Our Offers

For more Test and Measurement knowledge and tips, view all technical articles. Visit our resources
Keysight assumes no liability for the completeness, correctness and accuracy of all content on this website and all of its content. Please read here the terms of use of this website.