- Introduction
- Understanding Oscilloscope Probes and Their Significance
- The Role of Probes in Signal Measurements
- Benefits of Choosing Certified Refurbished Probes
- Financial Advantages: Quality at a Fraction of the Cost
- Quality and Reliability with Keysight's Certification
- Eco-Friendly and Sustainable Engineering Choices
- Top Features to Look for in Refurbished Oscilloscope Probes
- Warranty & Assurances
- Bandwidth and Frequency Range
- Probe Input Resistance and Capacitance
- Influencing Measurement Accuracy
- Probe Geometry and Ergonomics
- Compatibility and Integration with Oscilloscopes
- Keysight's Certification Process for Refurbished Probes
- Maintaining and Caring for Your Oscilloscope Probes
- Conclusion: Elevating Engineering Practices with Refurbished Probes
- Final Key Takeaway: Excellence in Every Signal with Keysight’s Probes
- Whenever You’re Ready, Here Are 5 Ways We Can Help You
Picture this: It's crunch time, and you're in the lab, analyzing critical signals for a groundbreaking project. Your team depends on accurate data. But as you run your tests, you notice discrepancies in your readings. The clock is ticking, and the pressure mounts.
Eventually, after hours of frustration and diagnostics, you trace the inconsistency back to — you guessed it — a subpar oscilloscope probe.
Have you ever grappled with signal discrepancies only to realize the reason was a faulty probe?
The heart of an oscilloscope's precision lies in its probes. These essential tools significantly influence signal integrity and measurement accuracy.
Investing in a top-tier oscilloscope only to pair it with a substandard probe can compromise the entire setup, leading to inaccuracies, distorted signals, and wasted hours in troubleshooting. Such challenges underscore the importance of choosing quality probes.
Certified refurbished Keysight oscilloscope probes present a compelling solution. They combine reliability with affordability, ensuring optimal performance. Setting the foundation right ensures your measurements remain accurate and consistent.
Join us as we delve into the advantages of these refurbished treasures, ensuring your readings always hit the mark.
Understanding Oscilloscope Probes and Their Significance
Oscilloscope probes serve as the primary bridge between your electronic device under test (DUT) and the oscilloscope itself. They play a crucial role in capturing and transmitting signals without introducing distortion or interference.
The Role of Probes in Signal Measurements
At its core, an oscilloscope probe's mission is to convey an electrical signal from the DUT to the oscilloscope's input. However, this transfer isn't always straightforward.
The probe can introduce capacitance, resistance, and inductance, which can subtly or significantly modify the signal. Hence, understanding and managing these nuances becomes essential for accurate readings.
Types of Probes
Modern electrical engineering presents various challenges, necessitating a diverse range of oscilloscope probes. Some of the key types include:
- Passive probes: Ideal for low-frequency applications.
- Active probes: Designed specifically for high-frequency signals.
- Differential probes: Useful in measuring the voltage difference between two points.
- Current probes: Created to detect current flow.
Understanding the unique strengths and applications of each probe type can greatly enhance your measurement approach.
The Importance of Quality
A top-tier oscilloscope probe ensures minimal interference with the signal it measures. By maintaining the integrity of the signal, quality probes provide confidence in your readings. Conversely, inferior probes can lead to signal degradation, resulting in inaccuracies and potential misinterpretations.
Three common mistakes and how to avoid them:
- Using the wrong probe type for a specific application: Just as tools differ, probes aren't one-size-fits-all. Using a passive probe for high-frequency applications, for instance, will lead to imprecise readings.
- Solution: Match the probe type to your measurement needs.
- Overlooking probe calibration: Probes might drift from their specified performance over time.
- Solution: Calibrate your probes regularly. Most modern oscilloscopes offer built-in calibration routines.
- Neglecting grounding issues: Poor grounding can add noise to your measurements.
- Solution: Keep your probe's ground lead short and ensure a secure connection to an appropriate ground.
While oscilloscopes often receive much attention, probes are the unsung heroes in signal measurement. Prioritizing quality and understanding probe selection and maintenance can significantly impact your engineering outcomes.
Find Certified Refurbished Probes On Sale Now
Benefits of Choosing Certified Refurbished Probes
When it comes to precision and reliability in measurements, the right probe can make all the difference. Certified refurbished probes, particularly from renowned brands like Keysight, present a compelling package of benefits for discerning engineers. Let's delve into the key advantages:
- Cost-effectiveness: Enjoy a wide range of quality equipment without breaking the bank.
- Quality assurance: Rest assured, each probe has passed rigorous testing and meets high-quality standards.
- Environmental benefits: Make a positive impact on the planet by reducing e-waste and promoting sustainability.
Financial Advantages: Quality at a Fraction of the Cost
Refurbished probes offer the same stellar performance as their brand-new counterparts but come at a significantly reduced cost. Engineers and companies can save substantially, freeing up budget for other crucial resources or additional tools. The cost-saving doesn't mean a compromise on quality; it's about smart spending without sacrificing performance.
Quality and Reliability with Keysight's Certification
Keysight's refurbishment process is comprehensive, ensuring that each piece of equipment, including probes, not only functions flawlessly but also appears in top-notch condition.
Keysight refurbishes probes at their own facilities, ensuring that each piece of equipment receives the attention and expertise it deserves. This in-house process allows for unparalleled oversight, ensuring that every probe meets the company's rigorous standards.
When you opt for a refurbished probe from Keysight, you aren't compromising on quality. You're investing in a piece of equipment that has been meticulously restored, updated, and optimized for modern engineering tasks.
Eco-Friendly and Sustainable Engineering Choices
In today's era, where sustainability is more than just a buzzword, choosing refurbished probes embodies responsible decision-making. Opting for refurbished equipment directly contributes to reducing e-waste, a significant environmental concern.
As industries churn out new devices at breakneck speed, the pile of discarded electronics grows. By supporting and promoting the refurbishment market, not only do engineers get top-tier equipment, they also play a part in crafting a greener future, making it a win-win scenario for both the planet and the profession.

Top Features to Look for in Refurbished Oscilloscope Probes
When considering a refurbished oscilloscope probe, especially from a trusted brand like Keysight, certain features stand out as essential.
The table below provides a comparative analysis of these crucial features, their significance in the engineering domain, and what one can expect from a certified refurbished probe from Keysight.
Feature | Importance | Keysight's Refurbished Probes |
Calibration | Ensures accuracy and reliability in measurements. | Calibrated to stringent standards with a certificate provided, ensuring precision and trust. |
Physical Condition | A good physical state indicates careful refurbishment and affects the user experience. | Almost indistinguishable from new probes due to comprehensive cleaning and parts replacement. |
Bandwidth & Range Verification | Confirms the probe's ability to measure across the expected spectrum accurately. | Keysight verifies that each probe meets or exceeds its original specifications. |
Warranty | Offers protection against unexpected failures and instills confidence in the purchase. | Comes with the same warranty as a new Keysight instrument, ensuring peace of mind. |
101-Point Inspection | Ensures every facet of the probe has been checked for functionality and quality. | Each unit undergoes this rigorous inspection, guaranteeing reliability and top-tier performance. |
Warranty & Assurances
The decision to invest in an oscilloscope probe, particularly a used or refurbished one, shouldn't be taken lightly. After all, the quality of the probe directly influences the precision of your measurements. This is where warranties and assurances come into play.
Importance of Warranty
A warranty isn't just a piece of paper; it's a commitment from the manufacturer or seller regarding the quality and reliability of the product. Most probes, especially refurbished ones, come with a 90-day warranty as standard.
This duration provides users with ample time to test and ensure the product performs as expected. However, with certain brands or upon request, this warranty can be extended up to 5 years. An extended warranty offers:
- Peace of mind: Knowing that your investment is protected for a longer duration allows you to focus on your work without concerns about equipment malfunction.
- Savings in the long run: If a malfunction does occur, warranty coverage can save significant repair or replacement costs.
- Indication of quality: A longer warranty often signifies the manufacturer's confidence in the product's durability and longevity.
KeysightCare vs. Non-Certified Sources
When you choose a brand like Keysight, you're not just getting a product; you're entering into a partnership. With KeysightCare, you receive:
- Dedicated technical support: Have access to experts who can assist with any technical challenges or questions.
- Faster repair times: In the unlikely event of a malfunction, Keysight prioritizes your product's repair.
- Comprehensive coverage: Beyond just the probe, the warranty often covers crucial accessories and parts.
In contrast, buying from non-certified sources can be a gamble. While you might land a good deal, there's no assurance of the product's history, how it was used, or if it was properly maintained. Without proper certification, you risk investing in a tool that might not deliver the expected performance.
Bandwidth and Frequency Range
For any engineer, the specifications of their tools aren't mere numbers but determinants of what they can achieve with them. With oscilloscope probes, bandwidth and frequency range hold paramount importance.
Relevance of Bandwidth and Frequency
The bandwidth of an oscilloscope probe indicates the range of frequencies it can accurately measure. It's a crucial specification because:
- Diverse applications: Engineers working on high-speed digital systems need probes with a higher bandwidth compared to those working on audio-frequency projects.
- Accuracy of measurements: A probe's bandwidth should be higher than the maximum frequency you intend to measure. Otherwise, the measurements can be attenuated or distorted.
- Future-proofing: Investing in a probe with a higher bandwidth than currently needed ensures it remains relevant for future projects or advancements in your field.
Adapting to Engineering Needs
Different engineering fields have varying frequency requirements. For instance:
- Digital system designers: Often require higher bandwidth probes to measure fast-changing signals accurately.
- Power electronics engineers: Might prioritize probes that can handle higher voltages over those with extreme bandwidths.
- Communication engineers: Need probes that can accurately capture modulated signals, which might have frequency components spread across a wide spectrum.
In essence, the bandwidth and frequency range of an oscilloscope probe should align with your current and anticipated engineering applications. Making a well-informed choice ensures that the probe serves as a reliable partner in your explorations and innovations.
Probe Input Resistance and Capacitance
Oscilloscope probes are more than just connectors; they play a vital role in determining the quality and accuracy of the measurements you obtain.
Two essential parameters that define a probe's performance are its input resistance and capacitance.
Why These Parameters Matter
- Minimizing loading effects: A high input resistance is desirable because it minimizes the loading effect on the circuit under test. A higher resistance ensures that the probe draws minimal current from the circuit, preserving its original behavior.
- Reducing signal distortion: The input capacitance of a probe should ideally be low to reduce any potential distortion or attenuation of high-frequency signals. A higher input capacitance can create a low-pass filter effect with the circuit's resistance, limiting the bandwidth.
Influencing Measurement Accuracy
- True representation: A probe with optimal input resistance and capacitance values ensures that the waveform displayed on the oscilloscope represents the actual signal in the circuit.
- Avoiding phase shifts: Especially at higher frequencies, the reactive effects of capacitance can introduce phase shifts, which can alter time-related measurements.
A probe's input resistance and capacitance are critical for ensuring that the measurements you get are both accurate and representative of the actual conditions in the circuit.

Probe Geometry and Ergonomics
While the technical specifications of a probe are undoubtedly crucial, the physical design and ergonomics also play a significant role in determining its utility and the user's experience.
Importance of Probe Geometry
- Access to tight spots: Modern electronic devices are becoming increasingly compact. A probe with a slim and precise tip geometry can access test points in tight or crowded areas without shorting adjacent components.
- Stability and precision: A well-designed probe tip can ensure stability when connected, reducing potential errors from intermittent contacts.
Ergonomics and User Experience
- Comfortable handling: If you're an engineer or technician spending hours taking measurements, the comfort of the probe's grip can make a significant difference.
- Reduced fatigue: Probes designed with user ergonomics in mind can reduce hand fatigue, allowing for longer testing sessions without discomfort.
- Ease of adjustment: Features like a retractable hook or easily adjustable ground lead simplify the measurement process and enhance accuracy.
Influencing Measurement Precision
- Consistent contact: Ergonomically designed probes ensure consistent contact with the test point, reducing measurement variations.
- Reduced noise: A stable connection can minimize noise due to movement, ensuring cleaner and more accurate readings.
In essence, while the inner workings and specifications of a probe are of utmost importance, its external design and ergonomics can significantly impact both the user's experience and the quality of the measurements obtained.
Compatibility and Integration with Oscilloscopes
When using oscilloscope probes, compatibility isn't just a convenience—it's a necessity. Pairing the right probe with the right oscilloscope ensures optimal performance, precise readings, and a seamless user experience.
Why Compatibility Matters
- Optimal performance: Just as you wouldn't pair a high-performance sports car engine with an economy car transmission, using a mismatched probe and oscilloscope can limit the capabilities of both.
- Feature integration: Many modern oscilloscopes have advanced features that require specific probes to function correctly. Without the right probe, you might miss out on these functionalities.
- Safety considerations: Using incompatible probes can lead to inaccurate readings, which can be especially hazardous in high-voltage or high-frequency applications.
Benefits of Pairing with Keysight Oscilloscopes
- Seamless integration: Keysight oscilloscopes and probes are designed to work together, ensuring that you can access and utilize all features without hiccups.
- Guaranteed performance: Using a Keysight probe with an oscilloscope ensures that you get the performance and bandwidth advertised, with no unexpected limitations.
- Simplified setup: Many Keysight oscilloscopes automatically detect the connected probe and adjust settings accordingly, simplifying setup and reducing potential errors.
Real-world Compatibility Issues and Solutions
- Mismatched bandwidth: An engineer using a high-bandwidth oscilloscope with a low-bandwidth probe might notice that the readings aren't capturing all the details of a fast signal.
- Solution: Always ensure that the probe's bandwidth matches or exceeds the oscilloscope's bandwidth for accurate readings.
- Connector incompatibility: A technician trying to use a probe with a different connector type than what the oscilloscope accepts could face physical connection challenges.
- Solution: Use adapter connectors or, ideally, select probes specifically designed for the oscilloscope in use.
- Inaccurate automatic settings: When connecting a generic probe to an advanced oscilloscope, the automatic settings like attenuation ratio might not be set correctly.
- Solution: Manually set the probe's attenuation ratio on the oscilloscope or use probes from the same brand that support automatic detection and configuration.
Ensuring compatibility between your oscilloscope probe and the oscilloscope itself isn't just about making connections easier—it's about guaranteeing the accuracy and reliability of every measurement you make. When you opt for a brand like Keysight, that assurance is built into the experience.
Dive into Keysight’s Collection of Certified Refurbished Probes
Keysight's Certification Process for Refurbished Probes
Keysight's commitment to excellence doesn't waver, whether dealing with brand-new equipment or refurbishing used units. Their rigorous certification process ensures that every refurbished probe—or any piece of equipment, be it oscilloscopes or other testing tools—adheres to the highest standards of quality and reliability.
Here's a step-by-step breakdown of their meticulous process:
1. Arrival at the hub: Every used unit first arrives at Keysight’s primary manufacturing site located in Penang, Malaysia, ensuring a consistent start to the refurbishment journey.
2. Initial condition check: Upon its arrival, each used unit undergoes a rigorous inspection. This step ensures professionals identify any wear, damage, or other issues that might affect the unit's performance.
3. Comprehensive cleaning: Using advanced vacuum-based technology, every probe undergoes an in-depth cleaning process. It's not just about making the equipment look good; it's about ensuring optimal functionality. If any part doesn't meet the cleanliness standard, Keysight replaces it.
4. Configuration and update: Once cleaned and inspected, the equipment gets updated with the latest compatible firmware and software. This ensures that the unit operates with the most recent technological advancements and provides consistent performance.
5. Customization: Keysight understands that engineering needs evolve. As such, during the refurbishment process, hardware options or software applications might be added or removed based on the specific customer order or market demands.
6. Calibration and safety checks: Accuracy is paramount in the world of electrical measurements. Each unit, therefore, undergoes thorough calibration and safety tests, ensuring it performs optimally and safely in every scenario.
7. Updated accessories and manuals: Every refurbished unit receives brand-new accessories and manuals, identical to what a new Keysight instrument would include. This ensures users have all the necessary resources at their disposal.
8. Final 101-point inspection: Before being approved for resale, each instrument undergoes a comprehensive performance verification, capped by a rigorous 101-point quality check. This final inspection ensures that every aspect of the equipment meets Keysight's high standards.
9. Standard like-new warranty: Quality assurance doesn't end when the unit leaves the factory. Each refurbished unit comes with a warranty identical to that of a new Keysight instrument, underscoring the brand's confidence in its refurbishment process.
10. Careful packaging and shipment: Finally, with everything checked and approved, the instrument and its accessories are meticulously packed, ensuring they reach the customer in impeccable condition.
Keysight's refurbishment and certification process transforms used units into instruments that rival brand-new ones in terms of performance, reliability, and value.

Maintaining and Caring for Your Oscilloscope Probes
Proper care and maintenance of your oscilloscope probes, whether brand new or refurbished, are crucial to ensure they deliver consistently accurate measurements throughout their lifespan.
Here are some best practices to keep in mind:
- Regular cleaning: Gently wipe the probe's tips using isopropyl alcohol and a soft cloth or swab. Avoid aggressive cleaning agents or abrasive materials, as these can damage the probe.
- Inspect before use: Before each use, visually inspect the probe for any signs of damage, wear, or contamination. Check for bent or broken tips, which can impact measurement accuracy.
- Proper storage: When not in use, store probes in their provided cases or hang them using probe hangers. Avoid coiling the cables too tightly, as this can damage the internal wiring.
- Avoid mechanical stress: Handle the probes gently, ensuring not to pull on the cable or bend the connector excessively. Secure probes using clips or holders when in use to minimize movement and stress.
- Mind the temperature: Avoid exposing probes to extreme temperatures. High temperatures can affect the probe's performance and decrease its lifespan.
- Regular calibration: Depending on frequency of use and the application's precision requirements, calibrate the probes regularly to maintain accuracy.
- Avoid overvoltage: Ensure you don't exceed the probe's voltage rating. Overvoltage can damage the probe and negatively impact its performance.
- Check compatibility: Always use probes with oscilloscopes they're compatible with to ensure optimal performance and prevent potential damage.
- Keep connectors clean: Dust and debris can accumulate on the connectors. Periodically clean them using appropriate solvents to maintain good electrical contact.
By following these maintenance tips and best practices, you can significantly extend the life of your refurbished oscilloscope probes, ensuring they remain a valuable asset in your measurement toolkit for years to come.
Conclusion: Elevating Engineering Practices with Refurbished Probes
In the constantly evolving world of electrical engineering, having reliable equipment is paramount. Refurbished oscilloscope probes offer a sustainable and cost-effective solution, ensuring that engineers can access top-tier equipment without the hefty price tag of brand-new units.
The meticulous refurbishment and certification process undertaken by Keysight ensures that every probe, whether new or refurbished, delivers consistent and accurate measurements. As we've seen, from the initial arrival of a used unit to its eventual shipment to customers, Keysight guarantees quality at every step.
Achieving unparalleled measurement accuracy doesn't mean one has to break the bank. With Keysight's certified refurbished probes, engineers can harness precision, reliability, and sustainability, all bundled in one package.
Final Key Takeaway: Excellence in Every Signal with Keysight’s Probes
When it comes to capturing and analyzing signals, every detail matters. And while the world of electrical engineering offers a plethora of choices, not all are created equal.
By choosing certified refurbished probes from a trusted name like Keysight, engineers position themselves at the forefront of precision and innovation. Excellence isn't just an aspiration—it's a guarantee with Keysight’s probes.
In each signal, in every measurement, and through every engineering challenge, Keysight stands as the partner of choice for those who prioritize accuracy and reliability.
Whenever You’re Ready, Here Are 5 Ways We Can Help You
- Browse our premium used network analyzers, oscilloscopes, signal analyzers and waveform generators.
- Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri - Talk to our sales support team by clicking the icon (bottom right corner) on every offer page
- Create an account to get price alerts and access to exclusive waitlists.
- Talk to your account manager about your specific needs.